I/O Stream STDLIB Configuration
Description
I/O Stream STDLIB Configuration.
Overview
The buffering mode is enabled by default in nano-lib meaning that the low-level write function is called only when a '
' is seen by the standard library. This module allows to disable the buffering feature and output the data as soon as possible.
Functions |
|
| void | sl_iostream_stdlib_disable_buffering (void) |
|
Disable standard library buffering.
|
|
Function Documentation
◆ sl_iostream_stdlib_disable_buffering()
| void sl_iostream_stdlib_disable_buffering | ( | void |
|
) |
Disable standard library buffering.