Secure element driver initialization

Description

Data Structures

struct psa_drv_se_context_t
Driver context structure.

Typedefs

typedef psa_status_t (* psa_drv_se_init_t ) ( psa_drv_se_context_t *drv_context, void *persistent_data, psa_key_location_t location)
A driver initialization function.
typedef uint64_t psa_key_slot_number_t
An internal designation of a key slot between the core part of the PSA Crypto implementation and the driver.

Typedef Documentation

◆ psa_drv_se_init_t

typedef psa_status_t (* psa_drv_se_init_t) ( psa_drv_se_context_t *drv_context, void *persistent_data, psa_key_location_t location)

A driver initialization function.

Parameters
[in,out] drv_context The driver context structure.
[in,out] persistent_data A pointer to the persistent data that allows writing.
location The location value for which this driver is registered. The driver will be invoked for all keys whose lifetime is in this location.
Return values
PSA_SUCCESS The driver is operational. The core will update the persistent data in storage.
Returns
Any other return value prevents the driver from being used in this session. The core will NOT update the persistent data in storage.

◆ psa_key_slot_number_t

typedef uint64_t psa_key_slot_number_t

An internal designation of a key slot between the core part of the PSA Crypto implementation and the driver.

The meaning of this value is driver-dependent.