psa_drv_se_context_t Struct Reference

Driver context structure.

#include <crypto_se_driver.h>

Public Member Functions

const void *const MBEDTLS_PRIVATE (persistent_data)
A read-only pointer to the driver's persistent data.
const size_t MBEDTLS_PRIVATE (persistent_data_size)
The size of persistent_data in bytes.
uintptr_t MBEDTLS_PRIVATE (transient_data)
Driver transient data.

Driver context structure.

Driver functions receive a pointer to this structure. Each registered driver has one instance of this structure.

Implementations must include the fields specified here and may include other fields.

Member Function Documentation

◆ MBEDTLS_PRIVATE() [1/3]

const void* const psa_drv_se_context_t::MBEDTLS_PRIVATE ( persistent_data )

A read-only pointer to the driver's persistent data.

Drivers typically use this persistent data to keep track of which slot numbers are available. This is only a guideline: drivers may use the persistent data for any purpose, keeping in mind the restrictions on when the persistent data is saved to storage: the persistent data is only saved after calling certain functions that receive a writable pointer to the persistent data.

The core allocates a memory buffer for the persistent data. The pointer is guaranteed to be suitably aligned for any data type, like a pointer returned by malloc (but the core can use any method to allocate the buffer, not necessarily malloc ).

The size of this buffer is in the persistent_data_size field of this structure.

Before the driver is initialized for the first time, the content of the persistent data is all-bits-zero. After a driver upgrade, if the size of the persistent data has increased, the original data is padded on the right with zeros; if the size has decreased, the original data is truncated to the new size.

This pointer is to read-only data. Only a few driver functions are allowed to modify the persistent data. These functions receive a writable pointer. These functions are:

  • psa_drv_se_t::p_init
  • psa_drv_se_key_management_t::p_allocate
  • psa_drv_se_key_management_t::p_destroy

The PSA Cryptography core saves the persistent data from one session to the next. It does this before returning from API functions that call a driver method that is allowed to modify the persistent data, specifically:

  • psa_crypto_init() causes a call to psa_drv_se_t::p_init, and may call psa_drv_se_key_management_t::p_destroy to complete an action that was interrupted by a power failure.
  • Key creation functions cause a call to psa_drv_se_key_management_t::p_allocate, and may cause a call to psa_drv_se_key_management_t::p_destroy in case an error occurs.
  • psa_destroy_key() causes a call to psa_drv_se_key_management_t::p_destroy.

◆ MBEDTLS_PRIVATE() [2/3]

const size_t psa_drv_se_context_t::MBEDTLS_PRIVATE ( persistent_data_size )

The size of persistent_data in bytes.

This is always equal to the value of the persistent_data_size field of the psa_drv_se_t structure when the driver is registered.

◆ MBEDTLS_PRIVATE() [3/3]

uintptr_t psa_drv_se_context_t::MBEDTLS_PRIVATE ( transient_data )

Driver transient data.

The core initializes this value to 0 and does not read or modify it afterwards. The driver may store whatever it wants in this field.