HFRCO Initialization

Description

Initialize the HFRCO oscillator.

Configure the frequency band of the HFRCO. The configuration define SL_DEVICE_INIT_HFRCO_BAND is used to configure the frequency. If using Simplicity Studio, this configuration header is also configurable through the Project Configurator, by selecting the "Device Init: HFRCO" configuration component.

Functions

sl_status_t sl_device_init_hfrco (void)
Initialize HFRCO.

Function Documentation

sl_device_init_hfrco()

sl_status_t sl_device_init_hfrco ( void )

Initialize HFRCO.

Configure the frequency band of the HFRCO. The configuration define SL_DEVICE_INIT_HFRCO_BAND is used to configure the frequency.

Returns
Status code
Return values
SL_STATUS_OK HFRCO initialized successfully