psa_drv_se_key_management_t Struct Reference

A struct containing all of the function pointers needed to for secure element key management.

#include <crypto_se_driver.h>

Public Member Functions

psa_drv_se_allocate_key_t MBEDTLS_PRIVATE (p_allocate)
Function that allocates a slot for a key.
psa_drv_se_validate_slot_number_t MBEDTLS_PRIVATE (p_validate_slot_number)
Function that checks the validity of a slot for a key.
psa_drv_se_import_key_t MBEDTLS_PRIVATE (p_import)
Function that performs a key import operation.
psa_drv_se_generate_key_t MBEDTLS_PRIVATE (p_generate)
Function that performs a generation.
psa_drv_se_destroy_key_t MBEDTLS_PRIVATE (p_destroy)
Function that performs a key destroy operation.
psa_drv_se_export_key_t MBEDTLS_PRIVATE (p_export)
Function that performs a key export operation.
psa_drv_se_export_key_t MBEDTLS_PRIVATE (p_export_public)
Function that performs a public key export operation.

A struct containing all of the function pointers needed to for secure element key management.

PSA Crypto API implementations should populate instances of the table as appropriate upon startup or at build time.

If one of the functions is not implemented, it should be set to NULL.

Member Function Documentation

◆ MBEDTLS_PRIVATE() [1/7]

psa_drv_se_allocate_key_t psa_drv_se_key_management_t::MBEDTLS_PRIVATE ( p_allocate )

Function that allocates a slot for a key.

◆ MBEDTLS_PRIVATE() [2/7]

psa_drv_se_validate_slot_number_t psa_drv_se_key_management_t::MBEDTLS_PRIVATE ( p_validate_slot_number )

Function that checks the validity of a slot for a key.

◆ MBEDTLS_PRIVATE() [3/7]

psa_drv_se_import_key_t psa_drv_se_key_management_t::MBEDTLS_PRIVATE ( p_import )

Function that performs a key import operation.

◆ MBEDTLS_PRIVATE() [4/7]

psa_drv_se_generate_key_t psa_drv_se_key_management_t::MBEDTLS_PRIVATE ( p_generate )

Function that performs a generation.

◆ MBEDTLS_PRIVATE() [5/7]

psa_drv_se_destroy_key_t psa_drv_se_key_management_t::MBEDTLS_PRIVATE ( p_destroy )

Function that performs a key destroy operation.

◆ MBEDTLS_PRIVATE() [6/7]

psa_drv_se_export_key_t psa_drv_se_key_management_t::MBEDTLS_PRIVATE ( p_export )

Function that performs a key export operation.

◆ MBEDTLS_PRIVATE() [7/7]

psa_drv_se_export_key_t psa_drv_se_key_management_t::MBEDTLS_PRIVATE ( p_export_public )

Function that performs a public key export operation.