ACMP_Init_TypeDef Struct ReferenceEMLIB > ACMP
ACMP initialization structure.
Definition at line 733
of file em_acmp.h
.
#include <
em_acmp.h
>
Data Fields | |
ACMP_Accuracy_TypeDef | accuracy |
uint32_t | biasProg |
bool | enable |
ACMP_HysteresisLevel_TypeDef | hysteresisLevel |
bool | inactiveValue |
ACMP_InputRange_TypeDef | inputRange |
uint32_t | vrefDiv |
Field Documentation
ACMP_Accuracy_TypeDef ACMP_Init_TypeDef::accuracy |
ACMP accuracy mode. Select the accuracy mode that matches the required current usage and accuracy requirement. Low accuracy consumes less current while high accuracy consumes more current.
Definition at line 771
of file em_acmp.h
.
Referenced by ACMP_Init().
uint32_t ACMP_Init_TypeDef::biasProg |
Bias current. See the ACMP chapter about bias and response time in the reference manual for details. Valid values are in the range 0-7.
Definition at line 748
of file em_acmp.h
.
Referenced by ACMP_Init().
bool ACMP_Init_TypeDef::enable |
If true, ACMP is enabled after configuration.
Definition at line 823
of file em_acmp.h
.
Referenced by ACMP_Init().
ACMP_HysteresisLevel_TypeDef ACMP_Init_TypeDef::hysteresisLevel |
bool ACMP_Init_TypeDef::inactiveValue |
Inactive value emitted by ACMP during warmup.
Definition at line 804
of file em_acmp.h
.
Referenced by ACMP_Init().
ACMP_InputRange_TypeDef ACMP_Init_TypeDef::inputRange |
Input range. Adjust this setting to optimize the performance for a given input voltage range.
Definition at line 763
of file em_acmp.h
.
Referenced by ACMP_Init().
uint32_t ACMP_Init_TypeDef::vrefDiv |
VDD division factor. VREFOUT = VREFIN * (VREFDIV / 63). Valid values are in the 0-63 range.
Definition at line 815
of file em_acmp.h
.
Referenced by ACMP_Init().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emlib/inc/
em_acmp.h