IADC_SingleInput_t Struct ReferenceEMLIB > IADC
IADC single input selection structure
Definition at line 748
of file em_iadc.h
.
#include <
em_iadc.h
>
Data Fields | |
bool | compare |
uint8_t | configId |
IADC_NegInput_t | negInput |
IADC_PosInput_t | posInput |
Field Documentation
bool IADC_SingleInput_t::compare |
Perform digital window comparison on the result from this entry.
Definition at line 752
of file em_iadc.h
.
Referenced by IADC_updateSingleInput().
uint8_t IADC_SingleInput_t::configId |
IADC_NegInput_t IADC_SingleInput_t::negInput |
Port/pin input for the negative side of the ADC.
Definition at line 749
of file em_iadc.h
.
Referenced by IADC_updateSingleInput().
IADC_PosInput_t IADC_SingleInput_t::posInput |
Port/pin input for the positive side of the ADC.
Definition at line 750
of file em_iadc.h
.
Referenced by IADC_updateSingleInput().
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emlib/inc/
em_iadc.h