CMU_LFXOInit_TypeDef Struct ReferenceEMLIB > CMU
LFXO initialization structure. Init values should be obtained from a configuration tool, app. note or xtal datasheet.
Definition at line
289
of file
em_cmu.h
.
#include <
em_cmu.h
>
Data Fields |
|
| bool | agcEn |
| uint8_t | capTune |
| bool | disOnDemand |
| bool | failDetEM4WUEn |
| bool | failDetEn |
| bool | forceEn |
| uint8_t | gain |
| bool | highAmplitudeEn |
| CMU_LfxoOscMode_TypeDef | mode |
| bool | regLock |
| CMU_LfxoStartupDelay_TypeDef | timeout |
Field Documentation
| bool CMU_LFXOInit_TypeDef::agcEn |
| uint8_t CMU_LFXOInit_TypeDef::capTune |
Internal capacitance tuning.
Definition at line
291
of file
em_cmu.h
.
Referenced by BSP_initClocks() , and CMU_LFXOInit() .
| bool CMU_LFXOInit_TypeDef::disOnDemand |
Disable on-demand requests.
Definition at line
298
of file
em_cmu.h
.
Referenced by CMU_LFXOInit() .
| bool CMU_LFXOInit_TypeDef::failDetEM4WUEn |
EM4 wakeup on failure enable.
Definition at line
296
of file
em_cmu.h
.
Referenced by CMU_LFXOInit() .
| bool CMU_LFXOInit_TypeDef::failDetEn |
Oscillator failure detection enable.
Definition at line
297
of file
em_cmu.h
.
Referenced by CMU_LFXOInit() .
| bool CMU_LFXOInit_TypeDef::forceEn |
| uint8_t CMU_LFXOInit_TypeDef::gain |
| bool CMU_LFXOInit_TypeDef::highAmplitudeEn |
| CMU_LfxoOscMode_TypeDef CMU_LFXOInit_TypeDef::mode |
| bool CMU_LFXOInit_TypeDef::regLock |
| CMU_LfxoStartupDelay_TypeDef CMU_LFXOInit_TypeDef::timeout |
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_cmu.h