IADC_InitScan_t Struct ReferenceEMLIB > IADC
IADC scan init structure
Definition at line 699
of file em_iadc.h
.
#include <
em_iadc.h
>
Data Fields | |
IADC_Alignment_t | alignment |
uint8_t | dataValidLevel |
bool | fifoDmaWakeup |
bool | showId |
bool | start |
IADC_TriggerAction_t | triggerAction |
IADC_TriggerSel_t | triggerSelect |
Field Documentation
IADC_Alignment_t IADC_InitScan_t::alignment |
uint8_t IADC_InitScan_t::dataValidLevel |
Data valid level before requesting DMA transfer.
Definition at line 702
of file em_iadc.h
.
Referenced by IADC_initScan().
bool IADC_InitScan_t::fifoDmaWakeup |
Wake-up DMA when FIFO reaches data valid level.
Definition at line 703
of file em_iadc.h
.
Referenced by IADC_initScan().
bool IADC_InitScan_t::showId |
Tag FIFO entry with scan table entry id.
Definition at line 701
of file em_iadc.h
.
Referenced by IADC_initScan().
bool IADC_InitScan_t::start |
IADC_TriggerAction_t IADC_InitScan_t::triggerAction |
IADC_TriggerSel_t IADC_InitScan_t::triggerSelect |
The documentation for this struct was generated from the following file:
- C:/repos/super_h1/platform/emlib/inc/
em_iadc.h