LFRCO_TypeDef Struct ReferenceDevices > LFRCO
LFRCO Register Declaration.
Definition at line
48
of file
efr32bg21_lfrco.h
.
#include <
efr32bg21_lfrco.h
>
Data Fields |
|
| __IOM uint32_t | CAL |
| __IOM uint32_t | CAL_CLR |
| __IOM uint32_t | CAL_SET |
| __IOM uint32_t | CAL_TGL |
| __IOM uint32_t | IEN |
| __IOM uint32_t | IEN_CLR |
| __IOM uint32_t | IEN_SET |
| __IOM uint32_t | IEN_TGL |
| __IOM uint32_t | IF |
| __IOM uint32_t | IF_CLR |
| __IOM uint32_t | IF_SET |
| __IOM uint32_t | IF_TGL |
| __IM uint32_t | IPVERSION |
| __IM uint32_t | IPVERSION_CLR |
| __IM uint32_t | IPVERSION_SET |
| __IM uint32_t | IPVERSION_TGL |
| __IOM uint32_t | LOCK |
| __IOM uint32_t | LOCK_CLR |
| __IOM uint32_t | LOCK_SET |
| __IOM uint32_t | LOCK_TGL |
| uint32_t | RESERVED0 [1U] |
| uint32_t | RESERVED1 [1U] |
| uint32_t | RESERVED10 [1U] |
| uint32_t | RESERVED2 [1015U] |
| uint32_t | RESERVED3 [1U] |
| uint32_t | RESERVED4 [1U] |
| uint32_t | RESERVED5 [1015U] |
| uint32_t | RESERVED6 [1U] |
| uint32_t | RESERVED7 [1U] |
| uint32_t | RESERVED8 [1015U] |
| uint32_t | RESERVED9 [1U] |
| __IM uint32_t | STATUS |
| __IM uint32_t | STATUS_CLR |
| __IM uint32_t | STATUS_SET |
| __IM uint32_t | STATUS_TGL |
| __IM uint32_t | SYNCBUSY |
| __IM uint32_t | SYNCBUSY_CLR |
| __IM uint32_t | SYNCBUSY_SET |
| __IM uint32_t | SYNCBUSY_TGL |
Field Documentation
| __IOM uint32_t LFRCO_TypeDef::CAL |
Calibration Register
Definition at line
52
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::CAL_CLR |
Calibration Register
Definition at line
72
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::CAL_SET |
Calibration Register
Definition at line
62
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::CAL_TGL |
Calibration Register
Definition at line
82
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::IEN |
Interrupt Enable Register
Definition at line
55
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::IEN_CLR |
Interrupt Enable Register
Definition at line
75
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::IEN_SET |
Interrupt Enable Register
Definition at line
65
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::IEN_TGL |
Interrupt Enable Register
Definition at line
85
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::IF |
Interrupt Flag Register
Definition at line
54
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::IF_CLR |
Interrupt Flag Register
Definition at line
74
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::IF_SET |
Interrupt Flag Register
Definition at line
64
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::IF_TGL |
Interrupt Flag Register
Definition at line
84
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::IPVERSION |
IP version
Definition at line
49
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::IPVERSION_CLR |
IP version
Definition at line
69
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::IPVERSION_SET |
IP version
Definition at line
59
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::IPVERSION_TGL |
IP version
Definition at line
79
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::LOCK |
Configuration Lock Register
Definition at line
57
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::LOCK_CLR |
Configuration Lock Register
Definition at line
77
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::LOCK_SET |
Configuration Lock Register
Definition at line
67
of file
efr32bg21_lfrco.h
.
| __IOM uint32_t LFRCO_TypeDef::LOCK_TGL |
Configuration Lock Register
Definition at line
87
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
50
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED1[1U] |
Reserved for future use
Definition at line
53
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED10[1U] |
Reserved for future use
Definition at line
83
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED2[1015U] |
Reserved for future use
Definition at line
58
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED3[1U] |
Reserved for future use
Definition at line
60
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED4[1U] |
Reserved for future use
Definition at line
63
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED5[1015U] |
Reserved for future use
Definition at line
68
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED6[1U] |
Reserved for future use
Definition at line
70
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED7[1U] |
Reserved for future use
Definition at line
73
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED8[1015U] |
Reserved for future use
Definition at line
78
of file
efr32bg21_lfrco.h
.
| uint32_t LFRCO_TypeDef::RESERVED9[1U] |
Reserved for future use
Definition at line
80
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::STATUS |
Status Register
Definition at line
51
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::STATUS_CLR |
Status Register
Definition at line
71
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::STATUS_SET |
Status Register
Definition at line
61
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::STATUS_TGL |
Status Register
Definition at line
81
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line
56
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::SYNCBUSY_CLR |
Synchronization Busy Register
Definition at line
76
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::SYNCBUSY_SET |
Synchronization Busy Register
Definition at line
66
of file
efr32bg21_lfrco.h
.
| __IM uint32_t LFRCO_TypeDef::SYNCBUSY_TGL |
Synchronization Busy Register
Definition at line
86
of file
efr32bg21_lfrco.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/
efr32bg21_lfrco.h