GPIO_PORT_TypeDef Struct ReferenceDevices
GPIO_P EFR32BG21 GPIO PORT.
Definition at line
42
of file
efr32bg21_gpio_port.h
.
#include <
efr32bg21_gpio_port.h
>
Data Fields |
|
| __IOM uint32_t | CTRL |
| __IM uint32_t | DIN |
| __IOM uint32_t | DOUT |
| __IOM uint32_t | MODEH |
| __IOM uint32_t | MODEL |
| uint32_t | RESERVED0 [1] |
| uint32_t | RESERVED1 [6] |
Field Documentation
| __IOM uint32_t GPIO_PORT_TypeDef::CTRL |
Port control
Definition at line
43
of file
efr32bg21_gpio_port.h
.
| __IM uint32_t GPIO_PORT_TypeDef::DIN |
data in
Definition at line
48
of file
efr32bg21_gpio_port.h
.
| __IOM uint32_t GPIO_PORT_TypeDef::DOUT |
data out
Definition at line
47
of file
efr32bg21_gpio_port.h
.
| __IOM uint32_t GPIO_PORT_TypeDef::MODEH |
mode high
Definition at line
46
of file
efr32bg21_gpio_port.h
.
| __IOM uint32_t GPIO_PORT_TypeDef::MODEL |
mode low
Definition at line
44
of file
efr32bg21_gpio_port.h
.
| uint32_t GPIO_PORT_TypeDef::RESERVED0[1] |
Reserved for future use
Definition at line
45
of file
efr32bg21_gpio_port.h
.
| uint32_t GPIO_PORT_TypeDef::RESERVED1[6] |
Reserved for future use
Definition at line
49
of file
efr32bg21_gpio_port.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/
efr32bg21_gpio_port.h