SEMAILBOX_HOST_TypeDef Struct ReferenceDevices > SEMAILBOX_HOST
SEMAILBOX_HOST Register Declaration.
Definition at line
52
of file
efr32bg21_semailbox.h
.
#include <
efr32bg21_semailbox.h
>
Data Fields |
|
| __IOM uint32_t | CONFIGURATION |
| SEMAILBOX_FIFO_TypeDef | FIFO [16U] |
| __IM uint32_t | RX_HEADER |
| __IM uint32_t | RX_PROT |
| __IM uint32_t | RX_STATUS |
| __IOM uint32_t | TX_HEADER |
| __IM uint32_t | TX_PROT |
| __IM uint32_t | TX_STATUS |
Field Documentation
| __IOM uint32_t SEMAILBOX_HOST_TypeDef::CONFIGURATION |
Configuration
Definition at line
60
of file
efr32bg21_semailbox.h
.
| SEMAILBOX_FIFO_TypeDef SEMAILBOX_HOST_TypeDef::FIFO[16U] |
RX/TX FIFO
Definition at line
53
of file
efr32bg21_semailbox.h
.
| __IM uint32_t SEMAILBOX_HOST_TypeDef::RX_HEADER |
RX Header
Definition at line
59
of file
efr32bg21_semailbox.h
.
| __IM uint32_t SEMAILBOX_HOST_TypeDef::RX_PROT |
RX Protection
Definition at line
57
of file
efr32bg21_semailbox.h
.
| __IM uint32_t SEMAILBOX_HOST_TypeDef::RX_STATUS |
RX Status
Definition at line
55
of file
efr32bg21_semailbox.h
.
| __IOM uint32_t SEMAILBOX_HOST_TypeDef::TX_HEADER |
TX Header
Definition at line
58
of file
efr32bg21_semailbox.h
.
| __IM uint32_t SEMAILBOX_HOST_TypeDef::TX_PROT |
TX Protection
Definition at line
56
of file
efr32bg21_semailbox.h
.
| __IM uint32_t SEMAILBOX_HOST_TypeDef::TX_STATUS |
TX Status
Definition at line
54
of file
efr32bg21_semailbox.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/
efr32bg21_semailbox.h