SE_Status_t Struct ReferenceEMLIB > SE
Definition at line
342
of file
em_se.h
.
Data Fields |
|
| uint32_t | bootStatus |
| SE_DebugStatus_t | debugStatus |
| uint32_t | hostFwVersion |
| bool | secureBootEnabled |
| uint32_t | seFwVersion |
Field Documentation
| uint32_t SE_Status_t::bootStatus |
Boot status code / error code (Bits [7:0]).
Definition at line
344
of file
em_se.h
.
Referenced by SE_getStatus() .
| SE_DebugStatus_t SE_Status_t::debugStatus |
| uint32_t SE_Status_t::hostFwVersion |
Host firmware version (if available).
Definition at line
348
of file
em_se.h
.
Referenced by SE_getStatus() .
| bool SE_Status_t::secureBootEnabled |
| uint32_t SE_Status_t::seFwVersion |
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_se.h