RFCRC_TypeDef Struct ReferenceDevices > RFCRC
RFCRC Register Declaration.
Definition at line
48
of file
efr32bg21_rfcrc.h
.
#include <
efr32bg21_rfcrc.h
>
Data Fields |
|
| __IOM uint32_t | CMD |
| __IOM uint32_t | CMD_CLR |
| __IOM uint32_t | CMD_SET |
| __IOM uint32_t | CMD_TGL |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | CTRL_CLR |
| __IOM uint32_t | CTRL_SET |
| __IOM uint32_t | CTRL_TGL |
| __IM uint32_t | DATA |
| __IM uint32_t | DATA_CLR |
| __IM uint32_t | DATA_SET |
| __IM uint32_t | DATA_TGL |
| __IOM uint32_t | EN |
| __IOM uint32_t | EN_CLR |
| __IOM uint32_t | EN_SET |
| __IOM uint32_t | EN_TGL |
| __IOM uint32_t | INIT |
| __IOM uint32_t | INIT_CLR |
| __IOM uint32_t | INIT_SET |
| __IOM uint32_t | INIT_TGL |
| __IOM uint32_t | INPUTDATA |
| __IOM uint32_t | INPUTDATA_CLR |
| __IOM uint32_t | INPUTDATA_SET |
| __IOM uint32_t | INPUTDATA_TGL |
| __IM uint32_t | IPVERSION |
| __IM uint32_t | IPVERSION_CLR |
| __IM uint32_t | IPVERSION_SET |
| __IM uint32_t | IPVERSION_TGL |
| __IOM uint32_t | POLY |
| __IOM uint32_t | POLY_CLR |
| __IOM uint32_t | POLY_SET |
| __IOM uint32_t | POLY_TGL |
| uint32_t | RESERVED0 [1015U] |
| uint32_t | RESERVED1 [1015U] |
| uint32_t | RESERVED2 [1015U] |
| __IM uint32_t | STATUS |
| __IM uint32_t | STATUS_CLR |
| __IM uint32_t | STATUS_SET |
| __IM uint32_t | STATUS_TGL |
Field Documentation
| __IOM uint32_t RFCRC_TypeDef::CMD |
Command Register
Definition at line
53
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::CMD_CLR |
Command Register
Definition at line
73
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::CMD_SET |
Command Register
Definition at line
63
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::CMD_TGL |
Command Register
Definition at line
83
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::CTRL |
Control Register
Definition at line
51
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::CTRL_CLR |
Control Register
Definition at line
71
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::CTRL_SET |
Control Register
Definition at line
61
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::CTRL_TGL |
Control Register
Definition at line
81
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::DATA |
CRC Data Register
Definition at line
56
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::DATA_CLR |
CRC Data Register
Definition at line
76
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::DATA_SET |
CRC Data Register
Definition at line
66
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::DATA_TGL |
CRC Data Register
Definition at line
86
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::EN |
Enable peripheral clock to this module
Definition at line
50
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::EN_CLR |
Enable peripheral clock to this module
Definition at line
70
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::EN_SET |
Enable peripheral clock to this module
Definition at line
60
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::EN_TGL |
Enable peripheral clock to this module
Definition at line
80
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::INIT |
CRC Initialization Value
Definition at line
55
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::INIT_CLR |
CRC Initialization Value
Definition at line
75
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::INIT_SET |
CRC Initialization Value
Definition at line
65
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::INIT_TGL |
CRC Initialization Value
Definition at line
85
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::INPUTDATA |
Input Data Register
Definition at line
54
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::INPUTDATA_CLR |
Input Data Register
Definition at line
74
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::INPUTDATA_SET |
Input Data Register
Definition at line
64
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::INPUTDATA_TGL |
Input Data Register
Definition at line
84
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::IPVERSION |
IP Version
Definition at line
49
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::IPVERSION_CLR |
IP Version
Definition at line
69
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::IPVERSION_SET |
IP Version
Definition at line
59
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::IPVERSION_TGL |
IP Version
Definition at line
79
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::POLY |
CRC Polynomial Value
Definition at line
57
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::POLY_CLR |
CRC Polynomial Value
Definition at line
77
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::POLY_SET |
CRC Polynomial Value
Definition at line
67
of file
efr32bg21_rfcrc.h
.
| __IOM uint32_t RFCRC_TypeDef::POLY_TGL |
CRC Polynomial Value
Definition at line
87
of file
efr32bg21_rfcrc.h
.
| uint32_t RFCRC_TypeDef::RESERVED0[1015U] |
Reserved for future use
Definition at line
58
of file
efr32bg21_rfcrc.h
.
| uint32_t RFCRC_TypeDef::RESERVED1[1015U] |
Reserved for future use
Definition at line
68
of file
efr32bg21_rfcrc.h
.
| uint32_t RFCRC_TypeDef::RESERVED2[1015U] |
Reserved for future use
Definition at line
78
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::STATUS |
Status Register
Definition at line
52
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::STATUS_CLR |
Status Register
Definition at line
72
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::STATUS_SET |
Status Register
Definition at line
62
of file
efr32bg21_rfcrc.h
.
| __IM uint32_t RFCRC_TypeDef::STATUS_TGL |
Status Register
Definition at line
82
of file
efr32bg21_rfcrc.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/
efr32bg21_rfcrc.h