GPIO_TIMERROUTE_TypeDef Struct ReferenceDevices
Definition at line
112
of file
efr32bg21_gpio.h
.
Data Fields |
|
| __IOM uint32_t | CC0ROUTE |
| __IOM uint32_t | CC1ROUTE |
| __IOM uint32_t | CC2ROUTE |
| __IOM uint32_t | CDTI0ROUTE |
| __IOM uint32_t | CDTI1ROUTE |
| __IOM uint32_t | CDTI2ROUTE |
| uint32_t | RESERVED0 [1U] |
| __IOM uint32_t | ROUTEEN |
Field Documentation
| __IOM uint32_t GPIO_TIMERROUTE_TypeDef::CC0ROUTE |
CC0 port/pin select
Definition at line
114
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_TIMERROUTE_TypeDef::CC1ROUTE |
CC1 port/pin select
Definition at line
115
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_TIMERROUTE_TypeDef::CC2ROUTE |
CC2 port/pin select
Definition at line
116
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_TIMERROUTE_TypeDef::CDTI0ROUTE |
CDTI0 port/pin select
Definition at line
117
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_TIMERROUTE_TypeDef::CDTI1ROUTE |
CDTI1 port/pin select
Definition at line
118
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_TIMERROUTE_TypeDef::CDTI2ROUTE |
CDTI2 port/pin select
Definition at line
119
of file
efr32bg21_gpio.h
.
| uint32_t GPIO_TIMERROUTE_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
120
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_TIMERROUTE_TypeDef::ROUTEEN |
TIMER0 pin enable
Definition at line
113
of file
efr32bg21_gpio.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/
efr32bg21_gpio.h