GPIO_CMUROUTE_TypeDef Struct ReferenceDevices
Definition at line
50
of file
efr32bg21_gpio.h
.
Data Fields |
|
| __IOM uint32_t | CLKIN0ROUTE |
| __IOM uint32_t | CLKOUT0ROUTE |
| __IOM uint32_t | CLKOUT1ROUTE |
| __IOM uint32_t | CLKOUT2ROUTE |
| uint32_t | RESERVED0 [2U] |
| __IOM uint32_t | ROUTEEN |
Field Documentation
| __IOM uint32_t GPIO_CMUROUTE_TypeDef::CLKIN0ROUTE |
CLKIN0 port/pin select
Definition at line
52
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_CMUROUTE_TypeDef::CLKOUT0ROUTE |
CLKOUT0 port/pin select
Definition at line
53
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_CMUROUTE_TypeDef::CLKOUT1ROUTE |
CLKOUT1 port/pin select
Definition at line
54
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_CMUROUTE_TypeDef::CLKOUT2ROUTE |
CLKOUT2 port/pin select
Definition at line
55
of file
efr32bg21_gpio.h
.
| uint32_t GPIO_CMUROUTE_TypeDef::RESERVED0[2U] |
Reserved for future use
Definition at line
56
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_CMUROUTE_TypeDef::ROUTEEN |
CMU pin enable
Definition at line
51
of file
efr32bg21_gpio.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/
efr32bg21_gpio.h