IADC_Init_t Struct ReferenceEMLIB > IADC
IADC init structure, common for single conversion and scan sequence.
Definition at line
629
of file
em_iadc.h
.
#include <
em_iadc.h
>
Data Fields |
|
| bool | debugHalt |
| uint16_t | greaterThanEqualThres |
| bool | iadcClkSuspend0 |
| bool | iadcClkSuspend1 |
| uint16_t | lessThanEqualThres |
| uint8_t | srcClkPrescale |
| uint8_t | timebase |
| uint16_t | timerCycles |
| IADC_Warmup_t | warmup |
Field Documentation
| bool IADC_Init_t::debugHalt |
| uint16_t IADC_Init_t::greaterThanEqualThres |
Digital window comparator greater-than or equal threshold.
Definition at line
642
of file
em_iadc.h
.
Referenced by IADC_init() .
| bool IADC_Init_t::iadcClkSuspend0 |
Suspend IADC_CLK until PRS0 trigger.
Definition at line
630
of file
em_iadc.h
.
Referenced by IADC_init() .
| bool IADC_Init_t::iadcClkSuspend1 |
Suspend IADC_CLK until PRS1 trigger.
Definition at line
631
of file
em_iadc.h
.
Referenced by IADC_init() .
| uint16_t IADC_Init_t::lessThanEqualThres |
Digital window comparator less-than or equal threshold.
Definition at line
643
of file
em_iadc.h
.
Referenced by IADC_init() .
| uint8_t IADC_Init_t::srcClkPrescale |
User requested source clock divider (prescale+1) which will be used if the calculated prescaler value is less.
Definition at line
639
of file
em_iadc.h
.
Referenced by IADC_init() .
| uint8_t IADC_Init_t::timebase |
IADC clock cycles (timebase+1) corresponding to 1us. Used as time reference for IADC delays, e.g. warmup. If the user sets timebase to 0, then IADC_Init() will calculate the timebase using the currently defined CMU clock setting for the IADC.
Definition at line
634
of file
em_iadc.h
.
Referenced by IADC_init() .
| uint16_t IADC_Init_t::timerCycles |
Number of ADC_CLK cycles per TIMER event.
Definition at line
641
of file
em_iadc.h
.
Referenced by IADC_init() .
| IADC_Warmup_t IADC_Init_t::warmup |
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/emlib/inc/
em_iadc.h