GPIO_USARTROUTE_TypeDef Struct ReferenceDevices
Definition at line
123
of file
efr32bg21_gpio.h
.
Data Fields |
|
| __IOM uint32_t | CLKROUTE |
| __IOM uint32_t | CSROUTE |
| __IOM uint32_t | CTSROUTE |
| uint32_t | RESERVED0 [1U] |
| __IOM uint32_t | ROUTEEN |
| __IOM uint32_t | RTSROUTE |
| __IOM uint32_t | RXROUTE |
| __IOM uint32_t | TXROUTE |
Field Documentation
| __IOM uint32_t GPIO_USARTROUTE_TypeDef::CLKROUTE |
CLK port/pin select
Definition at line
129
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_USARTROUTE_TypeDef::CSROUTE |
CS port/pin select
Definition at line
125
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_USARTROUTE_TypeDef::CTSROUTE |
CTS port/pin select
Definition at line
126
of file
efr32bg21_gpio.h
.
| uint32_t GPIO_USARTROUTE_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
131
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_USARTROUTE_TypeDef::ROUTEEN |
USART0 pin enable
Definition at line
124
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_USARTROUTE_TypeDef::RTSROUTE |
RTS port/pin select
Definition at line
127
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_USARTROUTE_TypeDef::RXROUTE |
RX port/pin select
Definition at line
128
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_USARTROUTE_TypeDef::TXROUTE |
TX port/pin select
Definition at line
130
of file
efr32bg21_gpio.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/
efr32bg21_gpio.h