GPIO_FRCROUTE_TypeDef Struct ReferenceDevices
Definition at line
59
of file
efr32bg21_gpio.h
.
Data Fields |
|
| __IOM uint32_t | DCLKROUTE |
| __IOM uint32_t | DFRAMEROUTE |
| __IOM uint32_t | DOUTROUTE |
| uint32_t | RESERVED0 [1U] |
| __IOM uint32_t | ROUTEEN |
Field Documentation
| __IOM uint32_t GPIO_FRCROUTE_TypeDef::DCLKROUTE |
DCLK port/pin select
Definition at line
61
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_FRCROUTE_TypeDef::DFRAMEROUTE |
DFRAME port/pin select
Definition at line
62
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_FRCROUTE_TypeDef::DOUTROUTE |
DOUT port/pin select
Definition at line
63
of file
efr32bg21_gpio.h
.
| uint32_t GPIO_FRCROUTE_TypeDef::RESERVED0[1U] |
Reserved for future use
Definition at line
64
of file
efr32bg21_gpio.h
.
| __IOM uint32_t GPIO_FRCROUTE_TypeDef::ROUTEEN |
FRC pin enable
Definition at line
60
of file
efr32bg21_gpio.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/super_h1/platform/Device/SiliconLabs/EFR32BG21/Include/
efr32bg21_gpio.h