Door Lock Server Callbacks
Functions | |
bool | emberAfPluginDoorLockServerActivateDoorLockCallback (bool activate) |
Activate Door Lock. |
Detailed Description
These callbacks are contributed by the Door Lock Server plugin.
Function Documentation
bool emberAfPluginDoorLockServerActivateDoorLockCallback | ( | bool | activate | ) |
This function is provided by the door lock server plugin.
- Parameters
-
activate
True if the lock should move to the locked position, false if it should move to the unlocked position Ver.: always
- Returns
- true if the callback was able to activate/deactivate the Lock.