Structure represents the enable/disable state of periodic advertising.
Public Attribute Documentation#
enable#
uint8_t ae_periodic_adv_enable::enable
uint8_t, enable, If this parameter is set Periodic Advertising starts 0 - Enable Periodic Advertising 1 - Include the ADI field in AUX_SYNC_IND PDUs
Definition at line
2024
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
adv_handle#
uint8_t ae_periodic_adv_enable::adv_handle
uint8_t, Advertising Handle, Used to identify an advertising set Range : 0x00 to 0xEF
Definition at line
2028
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h