Structure represents the BLE command to update connection parameters.

This structure is used to define the parameters for a BLE command to update connection parameters, which includes the address of the connected device, minimum and maximum connection intervals, peripheral latency, and supervision timeout.

Public Attributes#

uint8_t
uint16_t
uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_cmd_conn_params_update_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the connected device


Definition at line 969 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

min_interval#

uint16_t rsi_ble_cmd_conn_params_update_s::min_interval

Minimum connection interval


Definition at line 971 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

max_interval#

uint16_t rsi_ble_cmd_conn_params_update_s::max_interval

Maximum connection interval


Definition at line 973 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

latency#

uint16_t rsi_ble_cmd_conn_params_update_s::latency

Peripheral latency


Definition at line 975 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

timeout#

uint16_t rsi_ble_cmd_conn_params_update_s::timeout

Supervision timeout


Definition at line 977 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h