Structure represents the BLE Credit Based Flow Control (CBFC) data transmission.
This structure is used to define the parameters for a BLE CBFC data transmission, which includes the address of the remote device, the Local Channel Identifier (LCID), the length of the data to be transmitted, and the data to be transmitted.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_cbfc_data_tx_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the remote device
Definition at line
1095
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
lcid#
uint16_t rsi_ble_cbfc_data_tx_s::lcid
Local Channel Identifier (LCID)
Definition at line
1097
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
len#
uint16_t rsi_ble_cbfc_data_tx_s::len
Length of the data to be transmitted
Definition at line
1099
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
data#
uint8_t rsi_ble_cbfc_data_tx_s::data[RSI_DEV_ATT_LEN]
Data to be transmitted
Definition at line
1101
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h