Structure represents the BLE TX test mode parameters.
This structure is used to define the parameters for a BLE TX test mode, which includes the TX channel, PHY, length of the data to be transmitted, and data mode to be used for the test.
Public Attribute Documentation#
tx_channel#
uint8_t rsi_ble_tx_test_mode_s::tx_channel
TX channel to be used for the test
Definition at line
1145
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
phy#
uint8_t rsi_ble_tx_test_mode_s::phy
PHY to be used for the test
Definition at line
1147
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
tx_len#
uint8_t rsi_ble_tx_test_mode_s::tx_len
Length of the data to be transmitted
Definition at line
1149
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
tx_data_mode#
uint8_t rsi_ble_tx_test_mode_s::tx_data_mode
Data mode to be used for the test
Definition at line
1151
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h