Structure representing characteristic service data.

This structure is used to define the parameters for characteristic service data, including the characteristic value property, handle, and UUID.

Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

char_property#

uint8_t char_serv_data_s::char_property

Characteristic value property


reserved#

uint8_t char_serv_data_s::reserved

Reserved


char_handle#

uint16_t char_serv_data_s::char_handle

Characteristic value handle


char_uuid#

uuid_t char_serv_data_s::char_uuid

Characteristic value attributes UUID