Structure represents the BLE Security Manager Protocol (SMP) response.

This structure is used to define the parameters for a BLE SMP response, which includes the device address, IO capability, and Man-In-The-Middle (MITM) protection requirement.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_smp_response_s::dev_addr[RSI_DEV_ADDR_LEN]

Device address for the SMP response


Definition at line 846 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

io_capability#

uint8_t rsi_ble_smp_response_s::io_capability

IO capability of the device


Definition at line 848 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

mitm_req#

uint8_t rsi_ble_smp_response_s::mitm_req

MITM protection requirement


Definition at line 850 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h