Structure represents the BLE request to disconnect.
This structure is used to define the parameters for the BLE request to disconnect, which includes the device address, and the type of disconnect operation.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_req_disconnect_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the device to disconnect
Definition at line
781
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
type#
uint8_t rsi_ble_req_disconnect_s::type
Type of the disconnect operation
Definition at line
794
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h