Structure representing the BLE request to set LE ping timeout.
This structure is used to define the parameters for a BLE request to set the LE ping timeout, which includes the address of the connected device, and the LE ping timeout value to be set.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_set_le_ping_timeout_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the connected device
Definition at line
906
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
time_out#
uint16_t rsi_ble_set_le_ping_timeout_s::time_out
LE ping timeout value to be set
Definition at line
908
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h