Structure represents the BLE GATT read response.

This structure is used to define the parameters for a BLE GATT read response, which includes the remote device address, the type of the read response, reserved field for future use, the length of the attribute value, and the attribute value itself.

Public Attributes#

uint8_t
uint8_t
uint8_t
uint16_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_gatt_read_response_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address


Definition at line 1598 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

type#

uint8_t rsi_ble_gatt_read_response_s::type

Type of the read response


Definition at line 1600 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

reserved#

uint8_t rsi_ble_gatt_read_response_s::reserved

Reserved for future use


Definition at line 1602 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

data_len#

uint16_t rsi_ble_gatt_read_response_s::data_len

Attribute value length


Definition at line 1604 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

data#

uint8_t rsi_ble_gatt_read_response_s::data[RSI_DEV_ATT_LEN]

Attribute value (data)


Definition at line 1606 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h