Structure represents the remote BLE device information.
This structure is used to define the parameters for storing information about a remote BLE device, which includes its address, buffer counts, and synchronization mechanisms.
Public Attribute Documentation#
remote_dev_bd_addr#
uint8_t rsi_remote_ble_info_s::remote_dev_bd_addr[RSI_DEV_ADDR_LEN]
BD Address of the remote LE device
Definition at line
263
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
remote_dev_addr_type#
uint8_t rsi_remote_ble_info_s::remote_dev_addr_type
Address type of the remote LE device
Definition at line
265
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
avail_buf_cnt#
uint8_t rsi_remote_ble_info_s::avail_buf_cnt
Available Buffer Count
Definition at line
267
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
max_buf_cnt#
uint8_t rsi_remote_ble_info_s::max_buf_cnt
Max Buffer Count
Definition at line
269
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
max_buf_len#
uint16_t rsi_remote_ble_info_s::max_buf_len
Max Buffer Length
Definition at line
271
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
used#
uint8_t rsi_remote_ble_info_s::used
Flag for dev info used or not
Definition at line
273
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
cmd_in_use#
uint8_t rsi_remote_ble_info_s::cmd_in_use
Flag for checking command in use
Definition at line
275
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
expected_resp#
uint16_t rsi_remote_ble_info_s::expected_resp
Flag for checking expected remote response for each procedure
Definition at line
277
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
mode#
uint8_t rsi_remote_ble_info_s::mode
Buffer config mode
Definition at line
279
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h
ble_buff_mutex#
osMutexId_t rsi_remote_ble_info_s::ble_buff_mutex
Mutex handle for avail_buf_info update
Definition at line
281
of file components/device/silabs/si91x/wireless/ble/inc/rsi_bt_common.h