Structure represents the BLE GATT command to remove an attribute.
This structure is used to define the parameters for a BLE GATT command to remove an attribute, which includes the service handler and the attribute handle.
Public Attribute Documentation#
serv_hndler#
uint32_t rsi_ble_gatt_remove_att_s::serv_hndler
Service handler
Definition at line
1738
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
att_hndl#
uint16_t rsi_ble_gatt_remove_att_s::att_hndl
Attribute handle
Definition at line
1740
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h