Structure represents a BLE scan request.

Public Attributes#

uint8_t
uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

status#

uint8_t rsi_ble_req_scan_s::status

Scanning Status

  •   0 - disable 
    
  • 1 - enable


Definition at line 607 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

scan_type#

uint8_t rsi_ble_req_scan_s::scan_type

Scanning type

  • SCAN_TYPE_ACTIVE 0x01

  • SCAN_TYPE_PASSIVE 0x00


Definition at line 616 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

filter_type#

uint8_t rsi_ble_req_scan_s::filter_type

To filter incoming advertising reports

  • FILTERING_DISABLED = 0 (default)

  • ACCEPTLIST_FILTERING = 1 Note


Definition at line 627 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

own_addr_type#

uint8_t rsi_ble_req_scan_s::own_addr_type

Address type of the local device

  •   #define LE_PUBLIC_ADDRESS                  0x00 
    
  •   #define LE_RANDOM_ADDRESS                  0x01 
    
  •   #define LE_RESOLVABLE_PUBLIC_ADDRESS       0x02 
    
  •   #define LE_RESOLVABLE_RANDOM_ADDRESS       0x03  
    

Definition at line 642 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

scan_int#

uint16_t rsi_ble_req_scan_s::scan_int

Scan interval

  •  This is defined as the time interval from when the Controller started
     its last LE scan until it begins the subsequent LE scan. 
    
  •  Range: 0x0004 to 0x4000 
    

Definition at line 652 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

scan_win#

uint16_t rsi_ble_req_scan_s::scan_win

Scan window

  •   The duration of the LE scan. LE_Scan_Window should be less than or equal to LE_Scan_Interval 
    
  •   Range: 0x0004 to 0x4000 
    

Definition at line 661 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h