Structure represents the BLE RX test mode parameters.
This structure is used to define the parameters for a BLE RX test mode, which includes the RX channel, PHY, and modulation type to be used for the test.
Public Attribute Documentation#
rx_channel#
uint8_t rsi_ble_rx_test_mode_s::rx_channel
RX channel to be used for the test
Definition at line
1129
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
phy#
uint8_t rsi_ble_rx_test_mode_s::phy
PHY to be used for the test
Definition at line
1131
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
modulation#
uint8_t rsi_ble_rx_test_mode_s::modulation
Modulation type to be used for the test
Definition at line
1133
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h