Structure representing the BLE request for profiles list.

This structure is used to define the parameters for a BLE request to get the profiles list, which includes the remote device address, the handle from which the profiles search would start, and the handle at which the profiles search will stop.

Public Attributes#

uint8_t
uint16_t
uint16_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_req_profiles_list_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address


Definition at line 1211 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

start_handle#

uint16_t rsi_ble_req_profiles_list_s::start_handle

Profiles search will start from this handle


Definition at line 1213 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

end_handle#

uint16_t rsi_ble_req_profiles_list_s::end_handle

Profiles search will stop at this handle


Definition at line 1215 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h