You are viewing documentation for version:
Structure represents the BLE configuration for write without response notification buffer.
This structure is used to define the parameters for configuring the buffer for write without response notifications, which includes the remote device address, the buffer configuration mode, and the buffer count.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_set_wo_resp_notify_buf_info_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address
buf_mode#
uint8_t rsi_ble_set_wo_resp_notify_buf_info_s::buf_mode
Buffer config mode: 0 for small buffer mode, 1 for big buffer mode
buf_count#
uint8_t rsi_ble_set_wo_resp_notify_buf_info_s::buf_count
Buffer count