Structure represents the BLE CBFC (Credit Based Flow Control) disconnection.
This structure is used to define the parameters for a BLE CBFC disconnection, which includes the address of the remote device and the Local Channel Identifier (LCID).
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_cbfc_disconn_s::dev_addr[RSI_DEV_ADDR_LEN]
Address of the remote device
Definition at line
1114
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
lcid#
uint16_t rsi_ble_cbfc_disconn_s::lcid
Local Channel Identifier (LCID)
Definition at line
1116
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h