Structure representing the BLE request to manage the accept list using a payload.

This structure is used to define the parameters for the BLE request to manage the accept list, including the operation code, enable flag, total length of the payload, data compare index, length of the data to compare, and the advertising data payload.

Public Attributes#

uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

opcode#

uint8_t rsi_ble_req_acceptlist_using_payload_s::opcode[2]

Operation code for the request


Definition at line 535 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

enable#

uint8_t rsi_ble_req_acceptlist_using_payload_s::enable

Enable or disable the accept list


Definition at line 537 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

total_len#

uint8_t rsi_ble_req_acceptlist_using_payload_s::total_len

Total length of the payload


Definition at line 539 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

data_compare_index#

uint8_t rsi_ble_req_acceptlist_using_payload_s::data_compare_index

Index for comparing data


Definition at line 541 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

len_for_compare_data#

uint8_t rsi_ble_req_acceptlist_using_payload_s::len_for_compare_data

Length of the data to compare


Definition at line 543 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

adv_data_payload#

uint8_t rsi_ble_req_acceptlist_using_payload_s::adv_data_payload[31]

Advertising data payload


Definition at line 545 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h