Structure represents the BLE Advertising Extensions (AE) command to set a random address.
This structure is used to define the parameters for a BLE AE command to set a random address, which includes the advertising handle and the random address.
Public Attribute Documentation#
adv_handle#
uint8_t rsi_ble_ae_set_random_address_s::adv_handle
Advertising_Handle, used to identify an advertising set, Range: 0x00 to 0xEF
Definition at line
1820
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h
addr#
uint8_t rsi_ble_ae_set_random_address_s::addr[RSI_DEV_ADDR_LEN]
Random_Address, The Random Address may be of either Static Address or Private Address
Definition at line
1822
of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h