You are viewing documentation for version:
Structure represents the BLE request for characteristic services.
This structure is used to define the parameters for a BLE request to get characteristic services, which includes the remote device address, the handle from which the search will start, and the handle at which the search will end.
Public Attribute Documentation#
dev_addr#
uint8_t rsi_ble_req_char_services_s::dev_addr[RSI_DEV_ADDR_LEN]
Remote device address
start_handle#
uint8_t rsi_ble_req_char_services_s::start_handle[2]
Search will start from this handle
end_handle#
uint8_t rsi_ble_req_char_services_s::end_handle[2]
Search will end at this handle