Structure represents the BLE command to set a long attribute value.

This structure is used to define the parameters for a BLE command to set a long attribute value, which includes the remote device address, the attribute handle, the attribute value offset, the length of the attribute value, and the attribute value itself.

Public Attributes#

uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_set_long_att_val_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address


Definition at line 1425 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

handle#

uint8_t rsi_ble_set_long_att_val_s::handle[2]

Attribute handle


Definition at line 1427 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

offset#

uint8_t rsi_ble_set_long_att_val_s::offset[2]

Attribute value offset


Definition at line 1429 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

length#

uint8_t rsi_ble_set_long_att_val_s::length

Length of the attribute value


Definition at line 1431 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

att_value#

uint8_t rsi_ble_set_long_att_val_s::att_value[RSI_DEV_ATT_LEN]

Attribute value


Definition at line 1433 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h