Structure represents the BLE request to set the transmission power.

This structure is used to define the parameters for the BLE request to set the transmission power, which includes the transmission power value.

Public Attributes#

int8_t

Public Attribute Documentation#

tx_power#

int8_t rsi_ble_set_ble_tx_power_s::tx_power

Transmission power value


Definition at line 577 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h