Structure represents the BLE attribute error response.

This structure is used to define the parameters for a BLE event that involves an error response for an attribute operation from a remote device.

Public Attributes#

uint8_t
uint8_t
uint16_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_att_error_response_s::dev_addr[RSI_DEV_ADDR_LEN]

Address of the remote device


Definition at line 1710 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

req_opcode#

uint8_t rsi_ble_att_error_response_s::req_opcode

The request opcode for the BLE operation


Definition at line 1712 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

att_handle#

uint16_t rsi_ble_att_error_response_s::att_handle

The attribute handle for the Bluetooth Low Energy (BLE) device


Definition at line 1714 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

err_code#

uint8_t rsi_ble_att_error_response_s::err_code

The error code for the operation


Definition at line 1716 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h