Structure representing an attribute descriptor.

This structure is used to define the parameters for an attribute descriptor, including the attribute handle, reserved field, and attribute UUID.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

handle#

uint8_t att_desc_s::handle[2]

Attribute handle


Definition at line 601 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

reserved#

uint8_t att_desc_s::reserved[2]

Reserved


Definition at line 603 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h

att_type_uuid#

uuid_t att_desc_s::att_type_uuid

Attribute UUID (attribute type)


Definition at line 605 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble_apis.h