Structure represents the BLE request for a specific profile.

This structure is used to define the parameters for a BLE request to get a specific profile, which includes the remote device address, reserved bytes for future use, and the profile UUID.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_req_profile_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address


Definition at line 1228 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

reserved#

uint8_t rsi_ble_req_profile_s::reserved[2]

Reserved for future use


Definition at line 1230 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

profile_uuid#

uuid_t rsi_ble_req_profile_s::profile_uuid

Profile UUID (20 bytes)


Definition at line 1232 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h