You are viewing documentation for version:
Structure represents the BLE request to add a service.
This structure is used to define the parameters for a BLE request to add a service, which includes the service UUID, the number of attributes in the service, and the total size of the attributes' values (data).
Public Attribute Documentation#
service_uuid#
uuid_t rsi_ble_req_add_serv_s::service_uuid
Service UUID
num_of_attributes#
uint8_t rsi_ble_req_add_serv_s::num_of_attributes
Number of attributes in the service
total_att_datasize#
uint8_t rsi_ble_req_add_serv_s::total_att_datasize
Total size of the attributes' values (data)