Structure represents the BLE GATT write response.

This structure is used to define the parameters for a BLE GATT write response, which includes the remote device address and the response type.

Public Attributes#

uint8_t
uint8_t

Public Attribute Documentation#

dev_addr#

uint8_t rsi_ble_gatt_write_response_s::dev_addr[RSI_DEV_ADDR_LEN]

Remote device address


Definition at line 1619 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h

type#

uint8_t rsi_ble_gatt_write_response_s::type

Response type


Definition at line 1621 of file components/device/silabs/si91x/wireless/ble/inc/rsi_ble.h