Types
Event data types. More...
Enumerations |
|
| enum |
gos_event_flag_t
{
GOS_EVENT_FLAG_NONE = 0, GOS_EVENT_FLAG_RUN_NOW = (1 << 0), GOS_EVENT_FLAG_ALLOW_DUPLICATE = (1 << 1), GOS_EVENT_FLAG_REQUIRE_WLAN = (1 << 3), GOS_EVENT_FLAG_REQUIRE_SOFTAP = (1 << 4), GOS_EVENT_FLAG_REQUIRE_ETHERNET = (1 << 5), GOS_EVENT_FLAG_IN_EVENT_THREAD = (1 << 6), GOS_EVENT_FLAG_IN_NETWORK_WORKER = (1 << 7), GOS_EVENT_FLAG_UPDATE_TIMEOUT = (1 << 8) } |
|
Event flags.
More...
|
|
Detailed Description
Event data types.
Enumeration Type Documentation
◆ gos_event_flag_t
| enum gos_event_flag_t |
Event flags.
| Enumerator | |
|---|---|
| GOS_EVENT_FLAG_NONE |
No event flags set. |
| GOS_EVENT_FLAG_RUN_NOW |
Run the event immediately (should be used with gos_event_register_periodic() ) |
| GOS_EVENT_FLAG_ALLOW_DUPLICATE |
Allow duplicate event handler. |
| GOS_EVENT_FLAG_REQUIRE_WLAN |
The event won't execute unless the GOS_INTERFACE_WLAN interface is up. |
| GOS_EVENT_FLAG_REQUIRE_SOFTAP |
The event won't execute unless the GOS_INTERFACE_SOFTAP interface is up. |
| GOS_EVENT_FLAG_REQUIRE_ETHERNET |
The event won't execute unless the GOS_INTERFACE_ETHERNET interface is up. |
| GOS_EVENT_FLAG_IN_EVENT_THREAD |
The event will execute in the system event thread (.
|
| GOS_EVENT_FLAG_IN_NETWORK_WORKER |
The event will execute in the networking work thread. |
| GOS_EVENT_FLAG_UPDATE_TIMEOUT |
Update a timed event's timeout if it's currently pending. |