JSON parser configuration. More...
Data Fields |
|
| void * | buffer |
| uint16_t | buffer_len |
| gos_json_parse_reader_t | reader |
| gos_json_token_callback_t | token_callback |
|
Optional callback called before every token is allocated.
|
|
| gos_json_parse_flag_t | flags |
|
Parsing flags.
|
|
Detailed Description
JSON parser configuration.
This struct configures the JSON parsing context. It should be called with json_parse_context_init() to allocated a gos_json_parse_context_t context.
Field Documentation
◆ buffer
| void* gos_json_parse_config_t::buffer |
Optional, buffer containing pre-read data, or processing buffer for 'reader' if NULL then a processing buffer of size 'buffer_len' is allocated with the context
◆ buffer_len
| uint16_t gos_json_parse_config_t::buffer_len |
Length of buffer. This is either the length of pre-read JSON data or length of read's processing buffer.
◆ reader
| gos_json_parse_reader_t gos_json_parse_config_t::reader |
Optional, reader callback, continuously called by parser while there's more JSON data to be read, leave NULL if JSON data is pre-read and stored in 'buffer' member. Note: both 'buffer' and 'buffer_len' are required, they're passed as arguments to the 'reader' callback