PWM
Functions for using Pulse-Width-Modulation (PWM) peripheral. More...
Functions | |
gos_result_t | gos_pwm_update (gos_gpio_t gpio, uint32_t duty_cycle, uint32_t frequency) |
Enable/update PWM on specified GPIO. More... | |
gos_result_t | gos_pwm_stop (gos_gpio_t gpio) |
Disable PWM on specified GPIO. More... | |
Detailed Description
Functions for using Pulse-Width-Modulation (PWM) peripheral.
Function Documentation
◆ gos_pwm_stop()
gos_result_t gos_pwm_stop | ( | gos_gpio_t | gpio | ) |
Disable PWM on specified GPIO.
See Gecko OS Command API documentation: pwm_update.
- Parameters
-
[in] gpio
GPIO of corresponding PWM to disable
- Returns
- result of API, see gos_result_t
◆ gos_pwm_update()
gos_result_t gos_pwm_update | ( | gos_gpio_t | gpio, |
uint32_t | duty_cycle, |
||
uint32_t | frequency |
||
) |
Enable/update PWM on specified GPIO.
See Gecko OS Command API documentation: pwm_update.
- Note
- The
duty_cycle
argument is padded with 100 to enable finer resolution.
For example, a duty cycle of 34.78% would be 3478
.
- Parameters
-
[in] gpio
GPIO of corresponding PWM to enable/update [in] duty_cycle
duty cycle of PWM, padded with 100, 0-10000 (for 0.00 to 100.00%) [in] frequency
Frequency of PWM in Hz
- Returns
- result of API, see gos_result_t