Kernel Callbacks
Application functions that are called BY the Kernel. More...
Functions |
|
| void | gos_app_init (void) |
|
Application Initialization.
More...
|
|
| void | gos_app_deinit (void) |
|
Application De-initialization.
More...
|
|
| void | gos_app_idle (void) |
|
Application Idle.
More...
|
|
| void | gos_app_preinit (void) |
|
Application Pre-initialization.
More...
|
|
| void | gos_app_sram_init (void) |
|
RAM Initialization.
More...
|
|
Detailed Description
Application functions that are called BY the Kernel.
Function Documentation
◆ gos_app_deinit()
| void gos_app_deinit | ( | void |
|
) |
Application De-initialization.
This is called just before the application is shutdown by the Kernel. This is optional any may be omitted from the application.
This executes in the application thread.
- Examples:
- cloud/coap_demo/main.c , file/log_file/main.c , file/log_file_encrypted/main.c , hurricane/blinky/main.c , hurricane/marble/main.c , hurricane/weatherstation/main.c , intro/hello_world/main.c , manufacturing/factory_image/main.c , network/ethernet_bridge/main.c , peripheral/adc/main.c , system/system_monitor/main.c , test/certification/main.c , and test/hurricane/main.c .
◆ gos_app_idle()
| void gos_app_idle | ( | void |
|
) |
Application Idle.
This is called when there are no more pending events. This is optional any may be omitted from the application.
This executes in the application thread.
◆ gos_app_init()
| void gos_app_init | ( | void |
|
) |
Application Initialization.
This is the starting point for the application. This MUST be implemented in the application.
This executes in the application thread.
- Examples:
- cloud/coap_demo/main.c , cloud/dps_demo/main.c , cloud/mqtt_demo/main.c , demo/3d_demo/main.c , demo/accelerometer_stream/main.c , demo/secure_element/main.c , demo/uart_blaster/main.c , dms/messages/main.c , dms/ota_update/main.c , dms/telemetry/main.c , file/file_encrypt/main.c , file/file_list/main.c , file/log_file/main.c , file/log_file_encrypted/main.c , hurricane/arducam/main.c , hurricane/blinky/main.c , hurricane/gps/main.c , hurricane/marble/main.c , hurricane/security_camera/main.c , hurricane/weatherstation/main.c , intro/blinky/main.c , intro/hello_world/main.c , manufacturing/factory_image/main.c , network/ethernet_bridge/main.c , network/http_methods/main.c , network/http_server/main.c , network/http_server_stream/main.c , network/https_server/main.c , network/softap_tcp_server/main.c , network/tcp_client/main.c , network/tcp_echo_server/main.c , network/tcp_multiclient/main.c , network/uart_tcp_client/main.c , network/udp_client/main.c , network/udp_hello_gpio/main.c , network/websocket_client/main.c , network/websocket_cmd_stream/main.c , network/websocket_server/main.c , peripheral/adc/main.c , peripheral/button/main.c , peripheral/gpio_irq/main.c , security/aes_ctr/main.c , system/application_nvm/main.c , system/application_settings/main.c , system/core_dump/main.c , system/custom_commands/main.c , system/factory_reset_gpio/main.c , system/indicator/main.c , system/settings_file/main.c , system/system_monitor/main.c , system/uart/main.c , test/certification/main.c , test/ethernet/main.c , test/hurricane/main.c , test/spi_loop_back/main.c , test/throughput/main.c , test/uart_flow_control/main.c , utility/buffer_dump/main.c , utility/json_parser/main.c , utility/msgpack/main.c , utility/profiler/main.c , wifi/device_setup/main.c , wifi/web_setup/main.c , and wifi/wifi_scan/main.c .
◆ gos_app_preinit()
| void gos_app_preinit | ( | void |
|
) |
Application Pre-initialization.
This is called by the Kernel BEFORE the application is initialized. This is optional any may be omitted from the application.
This executes in the system thread.
- Note
- Extreme care should be used when implementing this function as it executes BEFORE the system is initialized.
- Examples:
- system/factory_reset_gpio/main.c .
◆ gos_app_sram_init()
| void gos_app_sram_init | ( | void |
|
) |
RAM Initialization.
This is called by the Kernel very early on in the application boot-up sequence. This initializes the application's .bss and .data sections. This is implemented internally by the SDK.
- Note
- WARN: This is for internal use only